16/11/2026
Murata Manufacturing Co., Ltd.
President: Christophe Pottier
Murata Manufacturing Co., Ltd. introduces the MGJ2T2 series of 2W SIP isolated gate-drive DC-DC converters for high-voltage silicon carbide (SiC) power applications. The new 2W series combines 6kVDC isolation with 2.5pF isolation capacitance and common-mode transient immunity (CMTI) exceeding 200kV/µs, supporting applications including energy storage and distribution, motor drives and EV charging.
The MGJ2T2 series operates from a 24V input and provides +18V/-3V bipolar outputs for SiC MOSFET gate drivers. The positive rail provides the voltage required to turn the power device on, while the negative rail supports reliable turn-off.
Fast switching in SiC-based power converters produces rapid voltage changes that can couple electrical noise across the isolation barrier between the power stage and its control circuitry. The low 2.5pF isolation capacitance of the MGJ2T2 series limits this coupling, while CMTI of more than 200kV/µs enables it to tolerate rapid common-mode voltage transitions. Together, these characteristics help maintain effective separation between the high-voltage switching environment and low-voltage control electronics.
Murata achieves this performance using its proprietary Block-Coil technology. Separate windings are formed on solid insulating formers, providing physical separation between the primary and secondary circuits while reducing the capacitance between them. The construction provides more than 8mm of creepage and clearance, while the solid insulation barrier provides high partial-discharge tolerance.
The MGJ2T2 series supports reinforced insulation at working voltages up to 800Vrms, or basic insulation up to 1600Vrms, and is tested to withstand 6kVDC across the isolation barrier. Designed to meet IEC 60664-1, which provides further assurance of the insulation system’s safety performance. These characteristics allow the gate-drive supply to operate where the control electronics and SiC power stage are at substantially different voltage potentials.
The same characteristics are relevant to emerging solid-state transformer (SST) architectures. SSTs use high-frequency power conversion and can divide high input voltages across multiple cascaded switching stages. Each switching element requires an isolated gate-drive power supply, making isolation and noise immunity between the individual power stages and their control circuitry particularly important.
The MGJ2T2 series operates over a temperature range of -40°C to +125°C and is supplied in an SIP package. Target applications include ESS and BESS, microgrids, motor drives, industrial automation, EV charging and heat pumps.
Murata in Brief
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.